Hello,
Has anyone suggestions for a moderately priced RF FSK Signal Generator with an external modulation input?
I need to simulate a very low cost, non-TI FSK transmitter in order to better understand the reaction of a CC1121 in receive mode.
The input to the generator is from a PIC microcontroller with a 1% internal oscillator.
It produces a Serial bit stream which has various "hiccups", jitter, drift, offset problems which need to be analyzed.
Minimum Requirements:
1GHZ Output
2-FSK @20KHz
4800BPS TTL Input
Thanks,