This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/LAUNCHXL-CC1310: Sensor Controller Studio: Button Debouncer Application and Low-Power Mode

Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310

Tool/software: TI-RTOS

Hello,

I am working with the Button Debouncer Example in Sensor Controller studio on the CC1310 Launchpad. I have taken the output files from Sensor Controller Studio and I am now using it through CCS.


The code comments indicate this is a low-power debouncer but my current measurements are at almost 4.9 mA. Do you know why these measurements are so high and what I can do either in Sensor Controller Studio or CCS to get a lower power reading?

 ler Studio