Part Number: LAUNCHXL-CC1350
Other Parts Discussed in Thread: CC1350, TIDEP0084
Tool/software: Linux
I'm trying to follow the Sub 1Ghz sensor to cloud Industrial Internet of Things Gateway out of the box Reference Design with the BeagleBone Black and CC1350 Launch Pad as MAC coprocessor.
I've been able to do all the steps up through 2.3.3 to start the application and the keep getting stuck on the run_demo.sh
it returns :command not found 46, :command not found 48, :command not found 49 and then line 96 :syntax error and unexpected end of line.
I have spent many hours reviewing everything. I have flashed the Launch Pad as coprocessor twice and hooked up to usb and device is recognized.
I have verified that the BBB booted off of SD card- saw Arago project loaded and was able to port the tidep0084 directory over.
I have changed the certs files and followed specific instructions for 2.3.3, but can't seem to move on.
I did not try the TI15.4 - Linux gateway project zero as I don't have an Ubuntu machine to load the TI 15.4 Stack Linux Gateway SDK.
Any help and support would be appreciated.
Thanks