Hi,
I've checked the IEEE MAC address of one our CC1310 Launchpads through Flash Programmer 2 and has the Flash Address of 0x500012F0, however, in the CCFG.h documentation (file:///C:/ti/simplelink_cc13x0_sdk_1_30_00_06/docs/driverlib_cc13xx_cc26xx/cc13x0/register_descriptions/CPU_MMAP/CCFG.html) it says there that the Flash Address of IEEE_MAC_0 is 0x5000 3FC8.
I also opened the ccfg.h and verified that it sayss the same as the documentation.
When I follow the declarations in the collector example, i see in hw_ccfg_simple_struct.h that the address there is the same as ccfg.h
Flash Programmer 2 | CCFG.h | |
IEE_MAC_0 | 0x500012F0 (Primary) | 0x00000FC8 |
IEE_MAC_1 | 0x0001FFC8 (Secondary) | 0x00000FCC |
From the Flash Programmer, when I scan the Primary Mac Address is says 00 12 4B 00 0E 09 30 B1
When I upload the collector example, and check the "ApiMac_extAddr" it says that the MAC Address is B1 30 9 0E 0 4B 12 0
1. Which one is the true address for the IEEE Mac Addresses?
2. Does each CC1310 have a unique IEEE MAC Address? (I've read they do so this is just for confirmation)
3. Which is really the mac address? Why is it reversed?