Part Number: CC1200
Hi,
One of my customer need some urgent help on CC1200 based RF module design. Design is already tested & crystal has become obsolete.
1. The external load capacitance calculation formula assumes stray capacitance from 2-5pF. Question is what assumption of stray capacitance to be made while selecting crystal. Having assumption of 2pF or 5pF makes difference of 6pF in external load capacitors. Is CC1200 robust enough to operate crystal correctly over range of external load capacitor. Kindly advice.
For ex. reference design of CC1200 has crystal of 10pF load capacitance & external capacitance of 15pF, so will the crystal as in below link work with CC1200. We are using 38.88MHz crystal & not 40MHz.
https://www.digikey.com/product-detail/en/txc-corporation/7M38872001/887-2549-1-ND/5725301
2. Also ESR of crystal (as mentioned above) is max 60E while datasheet of CC1200 also specified ESR of oscillator to be max. 60E. So question is do we need here some margin or 60E ESR crystal will work fine for our application.
3. Also in general what max frequency tolerance & stability I should look for reliable RF operation over operating range of -40’C to +85’C.