Other Parts Discussed in Thread: CC1350
I was reading about the 6lowpan network implementation.
Network consists of 2 important hardware parts 1. Nodes 2.Edge router
CC1350/ CC1310 could be used as a node.
As i read about edge router, it does following task
"The compressed IPv6 header needs an intermediary device to provide a conversion between 6LoWPAN and standard IP header and edge router is used for this"
But is it possible to use CC1350/ CC1310 as Edge router?
If yes, then how?
If no, then which devices are suitable for this task?