Other Parts Discussed in Thread: CC1101
Tool/software: TI-RTOS
Hello,
I'm currently developing on the CC1310 launch pad and the goal is a simplex RF link running at the highest possible speed. One CC1310 is always transmitting and the other receiving.
I'm trying to optimise the RF air time, or even have the transmitting CC1310 left in a constant carrier mode. To illustrate, I'm using the CC1310 rfPacketTx example in proprietary packet mode and I post two commands in back-to-back, however the CC1310 appears to turn off the transmitter between commands.
cmdHandle = RF_postCmd(rfHandle, (RF_Op*)&RF_cmdPropTx, RF_PriorityNormal, NULL, 0); cmdHandle = RF_postCmd(rfHandle, (RF_Op*)&RF_cmdPropTx, RF_PriorityNormal, NULL, 0);
I have this transmitting into my measurement device and its showing two transmit events:
Is there a way using the SDK or driver to eliminate the pause between transmissions? Or perhaps have the CC1310 in a constant carrier mode where it simply sends preamble when there are no RF commands to be executed?
Thanks,
Ben