Other Parts Discussed in Thread: TIDEP0084
Hi team,
I try to setup the TIDEP0084 (
) (Sub-1 GHz Sensor to Cloud Industrial IoT Gateway). But I meet the error of 'ENOTFOUND' like below. The BBB access Internet through one AP router with mobile SIM. So, there should be no firewall or proxy problem. (attachment is the fully log from BBB).
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.41-gf9f6f0db2d (gtbldadm@ubuntu-16) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 PREEMPT Wed Mar 29 17:37:15 EDT 2017
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x BeagleBone Black
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.0 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=5acae36b-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 459924K/524288K available (6603K kernel code, 317K rwdata, 2416K rodata, 264K init, 265K bss, 15212K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08d7004 (9021 kB)
[ 0.000000] .init : 0xc08d8000 - 0xc091a000 ( 264 kB)
[ 0.000000] .data : 0xc091a000 - 0xc09694b0 ( 318 kB)
[ 0.000000] .bss : 0xc09694b0 - 0xc09abbd8 ( 266 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000014] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000033] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000041] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000182] clocksource_probe: no matching clocksources found
[ 0.000337] Console: colour dummy device 80x30
[ 0.000359] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000365] This ensures that you still see kernel messages. Please
[ 0.000370] update your kernel commandline.
[ 0.000385] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.089239] pid_max: default: 32768 minimum: 301
[ 0.089350] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089360] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089967] Initializing cgroup subsys io
[ 0.089996] Initializing cgroup subsys memory
[ 0.090030] Initializing cgroup subsys devices
[ 0.090042] Initializing cgroup subsys freezer
[ 0.090055] Initializing cgroup subsys perf_event
[ 0.090064] Initializing cgroup subsys pids
[ 0.090090] CPU: Testing write buffer coherency: ok
[ 0.090453] Setting up static identity map for 0x80008200 - 0x80008260
[ 0.092248] devtmpfs: initialized
[ 0.102139] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.114667] omap_hwmod: debugss: _wait_target_disable failed
[ 0.170052] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.173564] pinctrl core: initialized pinctrl subsystem
[ 0.174746] NET: Registered protocol family 16
[ 0.176563] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.199233] cpuidle: using governor ladder
[ 0.229220] cpuidle: using governor menu
[ 0.232975] OMAP GPIO hardware version 0.1
[ 0.241462] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.276225] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.279429] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.279481] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c2_pins, deferring probe
[ 0.279596] media: Linux media interface: v0.10
[ 0.279662] Linux video capture interface: v2.00
[ 0.279705] pps_core: LinuxPPS API ver. 1 registered
[ 0.279711] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.279735] PTP clock support registered
[ 0.279787] EDAC MC: Ver: 3.0.0
[ 0.280801] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.281111] Advanced Linux Sound Architecture Driver Initialized.
[ 0.282092] clocksource: Switched to clocksource timer1
[ 0.291215] NET: Registered protocol family 2
[ 0.291887] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.291932] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.291970] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.292038] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.292054] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.292251] NET: Registered protocol family 1
[ 0.292617] RPC: Registered named UNIX socket transport module.
[ 0.292631] RPC: Registered udp transport module.
[ 0.292636] RPC: Registered tcp transport module.
[ 0.292642] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.293468] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.295113] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.301942] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.302826] NFS: Registering the id_resolver key type
[ 0.302891] Key type id_resolver registered
[ 0.302897] Key type id_legacy registered
[ 0.302958] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.306083] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.306110] io scheduler noop registered
[ 0.306121] io scheduler deadline registered
[ 0.306247] io scheduler cfq registered (default)
[ 0.307394] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.359641] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.363340] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 0.970968] console [ttyS0] enabled
[ 0.975383] [drm] Initialized drm 1.1.0 20060810
[ 0.986669] loop: module loaded
[ 0.991820] libphy: Fixed MDIO Bus: probed
[ 1.052159] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.058295] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[ 1.065343] libphy: 4a101000.mdio: probed
[ 1.069383] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[ 1.079299] cpsw 4a100000.ethernet: Detected MACID = c8:a0:30:ae:41:68
[ 1.086061] cpsw 4a100000.ethernet: cpts: overflow check period 850
[ 1.093971] mousedev: PS/2 mouse device common for all mice
[ 1.100096] i2c /dev entries driver
[ 1.104602] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.111995] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.193444] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.202849] NET: Registered protocol family 10
[ 1.208651] sit: IPv6 over IPv4 tunneling driver
[ 1.214131] NET: Registered protocol family 17
[ 1.218933] Key type dns_resolver registered
[ 1.223557] omap_voltage_late_init: Voltage driver support not added
[ 1.235603] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.245861] mmc0: new high speed SDHC card at address 0001
[ 1.251956] mmcblk0: mmc0:0001 TEAM 7.39 GiB
[ 1.258681] mmcblk0: p1 p2
[ 1.266605] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 1.274322] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.404408] tda998x 0-0070: found TDA19988
[ 1.409758] tilcdc 4830e000.lcdc: bound 0-0070 (ops tda998x_ops)
[ 1.415851] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.422541] [drm] No driver support for vblank timestamp query.
[ 1.428794] tilcdc 4830e000.lcdc: No connectors reported connected with modes
[ 1.435995] [drm] Cannot find any crtc or sizes - going 1024x768
[ 1.450530] Console: switching to colour frame buffer device 128x48
[ 1.462081] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.492179] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 1.498196] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.505207] at24 2-0054: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.512359] at24 2-0055: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.519416] at24 2-0056: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.526549] at24 2-0057: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.533528] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz
[ 1.541158] hctosys: unable to open rtc device (rtc0)
[ 1.549608] ALSA device list:
[ 1.552800] No soundcards found.
[ 1.665448] mmc1: MAN_BKOPS_EN bit is not set
[ 1.671728] mmc1: new high speed MMC card at address 0001
[ 1.677862] mmcblk1: mmc1:0001 MMC02G 1.79 GiB
[ 1.682708] mmcblk1boot0: mmc1:0001 MMC02G partition 1 1.00 MiB
[ 1.688868] mmcblk1boot1: mmc1:0001 MMC02G partition 2 1.00 MiB
[ 7.701765] EXT4-fs (mmcblk0p2): recovery complete
[ 7.802153] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 7.810417] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 7.823192] devtmpfs: mounted
[ 7.827079] Freeing unused kernel memory: 264K (c08d8000 - c091a000)
[ 7.833981] This architecture does not have kernel memory protection.
[ 8.208510] systemd[1]: System time before build time, advancing clock.
[ 8.293594] random: systemd: uninitialized urandom read (16 bytes read, 27 bits of entropy available)
[ 8.311354] random: systemd: uninitialized urandom read (16 bytes read, 27 bits of entropy available)
[ 8.334854] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 8.353906] systemd[1]: Detected architecture arm.
Welcome to Arago 2016.12!
[ 8.384361] systemd[1]: Set hostname to <am335x-evm>.
[ 8.485004] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 8.512605] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 8.527270] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 8.550545] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 31 bits of entropy available)
[ 8.581360] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 32 bits of entropy available)
[ 8.740894] random: systemd: uninitialized urandom read (16 bytes read, 36 bits of entropy available)
[ 8.751022] random: systemd: uninitialized urandom read (16 bytes read, 36 bits of entropy available)
[ 8.762009] random: systemd: uninitialized urandom read (16 bytes read, 36 bits of entropy available)
[ 9.092756] systemd[1]: [/lib/systemd/system/gadget-init.service:15] Unknown lvalue 'ExecStopPre' in section 'Service'
[ 9.454667] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
[ 9.462638] systemd[1]: sysinit.target: Found dependency on alignment.service/start
[ 9.470356] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
[ 9.477908] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
[ 9.487387] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start
[ SKIP ] Ordering cycle found, skipping alignment.service
[ 9.528043] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 9.553033] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 9.611609] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 9.642850] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 9.672852] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 9.702520] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 9.722683] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 9.752928] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 9.785443] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 9.813044] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 9.844324] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 9.878372] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 9.924636] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 9.957854] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 9.999801] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 10.057950] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 10.097550] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 10.157290] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 10.217557] systemd[1]: Starting Journal Service...
[ 10.244559] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
Starting Journal Service...
[ 10.301557] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 10.343528] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 10.382685] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.[ 10.388460] cryptodev: driver 1.8 loaded.
[ 10.414062] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 10.433195] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 10.472802] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 10.530755] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 10.552729] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 10.572624] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 10.593179] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
[ OK ] Started Setup Virtual Console.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Load Kernel Modules.
Starting Apply Kernel Variables...
Starting udev Coldplug all Devices...
Starting Create Static Device Nodes in /dev...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ 11.997568] systemd-journald[99]: Received request to flush runtime journal from PID 1
[ OK ] Started Flush Journal to Persistent Storage.
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Mounting /media/ram...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started udev Coldplug all Devices.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Load/Save Random Seed.
[ 13.793157] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 13.836728] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ 13.879373] 47401300.usb-phy supply vcc not found, using dummy regulator
[ OK ] Started Create Volatile Files and Directories.
[ 13.944180] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ OK ] Found device /dev/ttyS0.
[ 14.363908] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
Starting Update UTMP about System Boot/Shutdown...
Starting Network Time Synchronization...
[ OK ] Started Network Time Synchronization.
[ 15.169827] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 15.686476] remoteproc0: wkup_m3 is available
[ 15.690964] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 15.815352] ti-pruss 4a300000.pruss: creating PRU cores and other child platform devices
[ 15.840167] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 15.897598] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ 15.986155] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[ 16.075108] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 16.103669] remoteproc0: powering up wkup_m3
[ 16.109105] remoteproc0: Booting fw image am335x-pm-firmware.elf, size 217280
[ 16.143706] remoteproc1: 4a334000.pru0 is available
[ 16.148716] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 16.248341] remoteproc0: remote processor wkup_m3 is now up
[ 16.248358] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[ 16.316702] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 16.392803] [drm] Initialized pvr 1.14.3699939 20110701 on minor 1
[ 16.417724] remoteproc1: registered virtio0 (type 7)
[ 16.425758] PM: bootloader does not support rtc-only!
[ 16.466801] pru-rproc 4a334000.pru0: PRU rproc node /ocp/pruss@4a300000/pru0@4a334000 probed successfully
[ 16.498642] asoc-simple-card sound: i2s-hifi <-> 48038000.mcasp mapping ok
[ OK ] Found device /dev/ttyS3.
[ 16.562715] remoteproc2: 4a338000.pru1 is available
[ 16.567726] remoteproc2: Note: remoteproc is still under development and considered experimental.
[ 16.585292] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 16.663456] remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
Starting Synchronize System and HW clocks...
[ OK ] Reached target System Time Synchronized.
[ 16.848871] remoteproc2: registered virtio1 (type 7)
[ 16.879873] pru-rproc 4a338000.pru1: PRU rproc node /ocp/pruss@4a300000/pru1@4a338000 probed successfully
[ OK ] Started Synchronize System and HW clocks.
[ OK ] Found device /dev/mmcblk0p1.
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ OK ] Reached target System Initialization.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on dropbear.socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting Telephony service...
[ OK ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf.
Starting Print notice about GPLv3 packages...
[ OK ] Started System Logging Service.
[ OK ] Started D-Bus System Message Bus.
[ 18.515235] random: nonblocking pool is initialized
[ OK ] Started Telephony service.
Starting Network Service...
[ 18.777281] NET: Registered protocol family 15
Starting Permit User Sessions...
[ 18.858026] Bluetooth: Core ver 2.21
[ 18.861724] NET: Registered protocol family 31
Starting Start USB gadget...
[ OK ] Started Kernel Logging Service.
[ 19.006073] Bluetooth: HCI device and connection manager initialized
Starting Login Service...
[ 19.100347] Bluetooth: HCI socket layer initialized
Starting uim-sysfs.service...
Starting Avahi mDNS/DNS-SD Stack...
[ 19.178447] Bluetooth: L2CAP socket layer initialized
[ 19.248899] Bluetooth: SCO socket layer initialized
Starting Save/Restore Sound Card State...
[ OK ] Started Network Service.
[ OK ] Started Permit User Sessions.
[ 19.754861] net eth0: initializing cpsw version 1.12 (0)
[ 19.835978] net eth0: initialized cpsw ale version 1.4
[ OK ] Started Save/Restore Sound Card State.
[ 19.917615] net eth0: ALE Table size 1024
[ 19.999736] net eth0: phy found : id is : 0x7c0f1
[ 20.053937] Initializing XFRM netlink socket
[ 20.060058] libphy: PHY 4a101000.mdio:01 not found
[ 20.126247] net eth0: phy "4a101000.mdio:01" not found on slave 1, err -19
[ 20.256994] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[FAILED] Failed to start Start USB gadget.
See 'systemctl status gadget-init.service' for details.
[ 21.568646] usbcore: registered new interface driver usbfs
[ 21.678316] usbcore: registered new interface driver hub
[ 21.757392] usbcore: registered new device driver usb
[ 21.991367] musb-hdrc musb-hdrc.2.auto: MUSB HDRC host driver
[ 22.120009] musb-hdrc musb-hdrc.2.auto: new USB bus registered, assigned bus number 1
[ 22.238643] remoteproc1: powering up 4a334000.pru0
[ 22.246697] hub 1-0:1.0: USB hub found
[ 22.312962] hub 1-0:1.0: 1 port detected
[ 22.320011] remoteproc1: Booting fw image am335x-pru0-fw, size 75724
[ 22.409666] ti-pruss 4a300000.pruss: configured system_events = 0x0000000000030000 intr_channels = 0x00000005 host_intr = 0x00000005
[ 22.584537] remoteproc1: remote processor 4a334000.pru0 is now up
[ 22.643197] virtio_rpmsg_bus virtio0: creating channel rpmsg-pru addr 0x1e
[ 22.655338] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 22.706064] remoteproc2: powering up 4a338000.pru1
[ 22.741489] remoteproc2: Booting fw image am335x-pru1-fw, size 75724
[ 22.814950] ti-pruss 4a300000.pruss: configured system_events = 0x00000000000c0000 intr_channels = 0x0000000a host_intr = 0x0000000a
[ 22.852258] usb 1-1: new full-speed USB device number 2 using musb-hdrc
[ 22.929314] remoteproc2: remote processor 4a338000.pru1 is now up
[ 22.985212] virtio_rpmsg_bus virtio1: creating channel rpmsg-pru addr 0x1f
[ 22.995456] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 23.013139] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 23.098411] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 23.166488] rpmsg_pru rpmsg0: new rpmsg_pru device: /dev/rpmsg_pru30
[ 23.221819] rpmsg_pru rpmsg1: new rpmsg_pru device: /dev/rpmsg_pru31
[ 24.050690] cdc_acm 1-1:1.0: ttyACM0: USB ACM device
[ 24.112526] hid-generic 0003:0451:BEF3.0001: device has no listeners, quitting
[ 24.155754] cdc_acm 1-1:1.3: ttyACM1: USB ACM device
[ 24.163200] usbcore: registered new interface driver usbhid
[ 24.168811] usbhid: USB HID core driver
[ 24.195429] usbcore: registered new interface driver cdc_acm
[ 24.201136] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
binutils
bison-dev
bison
cpp-symlinks
cpp
dosfstools
g++-symlinks
g++
gawk-dev
gawk
gcc-symlinks
gcc
gdb
gdbserver
gstreamer1.0-libav
hidapi
libcairo-perf-utils
libgmp10
libidn11
libmpc3
libmpfr4
m4-dev
m4
make
nettle
swig-dev
swig
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started uim-sysfs.service.
[ OK ] Started Print notice about GPLv3 packages.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Login Service.
Mounting Configuration File System...
[ OK ] Reached target Sound Card.
Starting rc.pvr.service...
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Started Getty on tty1.
[ OK ] Reached target Network.[ 28.038894] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
Starting Network Name Resolution...
Starting Lightning Fast Webserver With Light System Requirements...
[ OK ] Mounted Configuration File System.
[ OK ] Started rc.pvr.service.
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
[ OK ] Started Network Name Resolution.
Starting weston.service...
[ OK ] Started weston.service.
Starting telnetd.service...
[ OK ] Started telnetd.service.
Starting thttpd.service...
Starting busybox-udhcpd.service...
[ OK ] Started thttpd.service.
[ OK ] Started busybox-udhcpd.service.
Starting rng-tools.service...
[ OK ] Started rng-tools.service.
Starting matrix-gui-2.0.service...
[ OK ] Started matrix-gui-2.0.service.
Starting thermal-zone-init.service...
Starting parse-ip.service...
[ OK ] Started thermal-zone-init.service.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyS0
Arago 2016.12 am335x-evm ttyS0
am335x-evm login: root
root@am335x-evm:~# cd AWS/prebuilt
root@am335x-evm:~/AWS/prebuilt# cd bin
root@am335x-evm:~/AWS/prebuilt/bin# ls
apimac-msgs.cfg collector.cfg host_collector nv-simulation.bin
bbb_collector collector.cfg_ori host_npi_server2 run_collector.sh
bbb_npi_server2 collector_log.txt npi_server2.cfg
root@am335x-evm:~/AWS/prebuilt/bin# vi collector.cfg
;The collector app can use either a socket or uart connection to the co-pr
;; Alternatively: 'interface = socket'
interface = uart
; Many of the "config-ITEMS" allow for direct configuration
; and overriding the 'config.h' default values
config-auto-start = true
config-channel-mask = 0
config-channel-page = 9
config-coord-short-addr = 0x1234
config-double-trickle-timer = false
config-dwell-time = 250
config-fh-async-channel-mask = all
config-fh-channel-mask = all
config-fh-enable = false
config-fh-netname = "FHTest"
config-fh-pan-size = 0x0032
config-linkquality = 1
config-mac-beacon-order = 15
config-mac-superframe-order = 15
config-pan-id = 0xAcDc
config-percentfilter = 0x0ff
config-phy-id = 3
config-scan-duration = 5
config-secure = true
config-trickle-max-clk-duration = 960000
config-trickle-min-clk-duration = 30000
; msg-dbg-data = apimac-msgs.cfg
root@am335x-evm:~/AWS/prebuilt/bin# cd ..
root@am335x-evm:~/AWS/prebuilt# ls
bin iot-gateway run_demo.sh
root@am335x-evm:~/AWS/prebuilt# cd ..
root@am335x-evm:~/AWS# cd prebuilt
root@am335x-evm:~/AWS/prebuilt# ls
bin iot-gateway run_demo.sh
root@am335x-evm:~/AWS/prebuilt# bash run_demo.sh
Launching the Collector Application in the background
Found Mac Co-Processor Version info is:
Transport: 3
Product: 1
Major: 2
Minor: 0
Maint: 0
----------------------------------------
Start the gateway application
Collector Running as Process id: 919
Launching Node-JS gateway application in background
Gateway is running as Process id: 931
root@am335x-evm:~/AWS/prebuilt# Connected to App Server
AWS Cloud Adapter error { [Error: getaddrinfo ENOTFOUND https://a23op339u3ex9t.iot.us-east-1.amazonaws.com https://a23op339u3ex9t.iot.us-east-1.amazonaws.com:8883]
code: 'ENOTFOUND',
errno: 'ENOTFOUND',
syscall: 'getaddrinfo',
hostname: 'https://a23op339u3ex9t.iot.us-east-1.amazonaws.com',
host: 'https://a23op339u3ex9t.iot.us-east-1.amazonaws.com',
port: 8883 }
AWS Cloud Adapter offline
AWS Cloud Adapter close
AWS Cloud Adapter reconnect
AWS Cloud Adapter error { [Error: getaddrinfo ENOTFOUND https://a23op339u3ex9t.iot.us-east-1.amazonaws.com https://a23op339u3ex9t.iot.us-east-1.amazonaws.com:8883]
code: 'ENOTFOUND',
errno: 'ENOTFOUND',
syscall: 'getaddrinfo',
hostname: 'https://a23op339u3ex9t.iot.us-east-1.amazonaws.com',
host: 'https://a23op339u3ex9t.iot.us-east-1.amazonaws.com',
port: 8883 }
AWS Cloud Adapter offline
AWS Cloud Adapter close
AWS Cloud Adapter reconnect
AWS Cloud Adapter error { [Error: getaddrinfo ENOTFOUND https://a23op339u3ex9t.iot.us-east-1.amazonaws.com https://a23op339u3ex9t.iot.us-east-1.amazonaws.com:8883]
code: 'ENOTFOUND',
errno: 'ENOTFOUND',
syscall: 'getaddrinfo',
hostname: 'https://a23op339u3ex9t.iot.us-east-1.amazonaws.com',
host: 'https://a23op339u3ex9t.iot.us-east-1.amazonaws.com',
port: 8883 }
AWS Cloud Adapter offline
AWS Cloud Adapter close
AWS Cloud Adapter reconnect
AWS Cloud Adapter error { [Error: getaddrinfo ENOTFOUND https://a23op339u3ex9t.iot.us-east-1.amazonaws.com https://a23op339u3ex9t.iot.us-east-1.amazonaws.com:8883]
code: 'ENOTFOUND',
errno: 'ENOTFOUND',
syscall: 'getaddrinfo',
hostname: 'https://a23op339u3ex9t.iot.us-east-1.amazonaws.com',
host: 'https://a23op339u3ex9t.iot.us-east-1.amazonaws.com',
port: 8883 }
AWS Cloud Adapter offline
AWS Cloud Adapter close
AWS Cloud Adapter reconnect
AWS Cloud Adapter error { [Error: getaddrinfo ENOTFOUND https://a23op339u3ex9t.iot.us-east-1.amazonaws.com https://a23op339u3ex9t.iot.us-east-1.amazonaws.com:8883]
code: 'ENOTFOUND',
errno: 'ENOTFOUND',
syscall: 'getaddrinfo',
hostname: 'https://a23op339u3ex9t.iot.us-east-1.amazonaws.com',
host: 'https://a23op339u3ex9t.iot.us-east-1.amazonaws.com',
port: 8883 }
AWS Cloud Adapter offline
AWS Cloud Adapter close
root@am335x-evm:~/AWS/prebuilt# bash run_demo.sh
Launching the Collector Application in the background
Found Mac Co-Processor Version info is:
Transport: 3
Product: 1
Major: 2
Minor: 0
Maint: 0
----------------------------------------
Start the gateway application
Collector Running as Process id: 919
Launching Node-JS gateway application in background
Gateway is running as Process id: 931
root@am335x-evm:~/AWS/prebuilt# Connected to App Server
AWS Cloud Adapter error { [Error: getaddrinfo ENOTFOUND https://a23op339u3ex9t.iot.us-east-1.amazonaws.com https://a23op339u3ex9t.iot.us-east-1.amazonaws.com:8883]
code: 'ENOTFOUND',
errno: 'ENOTFOUND',
syscall: 'getaddrinfo',
hostname: 'a23op339u3ex9t.iot.us-east-1.amazonaws.com',
host: 'a23op339u3ex9t.iot.us-east-1.amazonaws.com',
port: 8883 }
AWS Cloud Adapter offline
AWS Cloud Adapter close
AWS Cloud Adapter reconnect
I have tried to update certification file from stackarmor. But the error is the same.
I also tried to modify "config-phy-id=3" on collector.cfg. But this is no helpful.
Below is my setup.
Please help clarify. Thank you.