Part Number: CC1110-CC1111
Other Parts Discussed in Thread: TLV320AIC26, CC2510
I'm not able to sync master and slave I2S communication between two ,Sometimes the speech is perfect but it randomly fluctuates between good speech and bad speech.How can I possibly correct the syncing problem ?.I am able to speed up clock I2SCLKF1 = 0x57 and then reset to I2SCLKF1 = 0x59 for about 0.5 seconds and the toggling between good and bad speech happens,But how can I position the I2S syncing so that I able to get good speech every time.Please help me on understanding the problem and on why is it happening and how to solve it.
I'm referring "Application Note AN082 One-Way or Two-Way Audio Communications using the CC1110 or CC2510 and the TLV320AIC26 Codec" and my architecture is also the same only difference is the packet length..