This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200EMK-868-930: Tx Configuration Issues, trying to resolve

Part Number: CC1200EMK-868-930
Other Parts Discussed in Thread: CC1200DK

I am trying to generate the following waveform from the CC1200DK -

Waveform Target

  • Transmit Mode: Continuous (Infinite Packet Length)
  • RF: 868 MHz
  • Modulation Type: ASK/OOK
  • Modulation Depth: Full
  • Symbol Size: 12.5us

Issues

  • Transmit Mode
    • Continuous mode not working
  • Modulation Depth
    • With a sniffer I don't detect full CW-Off
  • Symbol Size
    • The values applied aren't working for me

  • Preamble
    • I have disabled the preamble but it still appears

In the attached project I observe a symbol size of 25.6us that doesn't hit 100% ASK_DEPTH. I have attached my project trying to achieve this, what is the best way for me to resolve these issues? I have spent SO much time here, reaching out to E2E for help! :)

Observed Waveform

  • Ch1(red) - P4.5
  • Ch2(yellow) - Base-band Sniffer (antenna and rectifier)

per test - cc1200 ASK demo.zip