Other Parts Discussed in Thread: CC1200DK
I am trying to generate the following waveform from the CC1200DK -
Waveform Target
- Transmit Mode: Continuous (Infinite Packet Length)
- RF: 868 MHz
- Modulation Type: ASK/OOK
- Modulation Depth: Full
- Symbol Size: 12.5us
Issues
- Transmit Mode
- Continuous mode not working
- Modulation Depth
- With a sniffer I don't detect full CW-Off
- Symbol Size
- The values applied aren't working for me
Observed Waveform
In the attached project I observe a symbol size of 25.6us that doesn't hit 100% ASK_DEPTH.
- Ch1(red) - P4.5
- Ch2(yellow) - Base-band Sniffer (antenna and rectifier)
I have attached my project trying to achieve this -
7457.per test - cc1200 ASK demo.zip
What is the best way for me to resolve these (3) issues? I have spent SO much time here, reaching out to E2E for help! :)