This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I want to ask a question about ccsv5 installing on ubuntu 14.04.
I have a problem. When i want to install ccsv5 on my computer i use offline installer. After 1,5 hours of installation it shows me "One or more features were not install correctly". I've cleaned installation directory manually, including installjamer. Then i repeated procedure, all the same. Please could anyone tell me what am i doing wrong. (CCSV5 5.1.2, My os is ubuntu 14.04). It also creates xml files with error logs.
I've also installed libraries, as was shown on ti wiki.
I tried reinstall newer versions (ccsv6) and get the same problem.