Other Parts Discussed in Thread: CC1310, CC1350
Tool/software: Code Composer Studio
I have my own board with cc1310 device on it. i was able to load the program on the device and run it properly earlier. Suddenly, I started seeing the error message:
Error connecting to the target:
(Error -241 @ 0x0)
A router subpath could not be accessed.
A security error has probably occurred.
Make sure your device is unlocked.
(Emulation package 6.0.628.1)
Using smart rf flash programmer 2, i tried mass erase of the flash. It says mass erase of flash is successful but i am still unable to the program the device. Another thing that i observed was that when the device was working properly smartRF flash programmer detected the device as cc1310. After the device started showing an error message it is being detected as cc1350.