This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: how can to increase throughput at 15.4 stack

Part Number: LAUNCHXL-CC1310


hi all,

how can to increase throughput when multi devices

now,i need to increase throughput event some devices power down ?

First, to change the  "INDIRECT_PERSISTENT_TIME"  when some device lost

1.

how can change the indirect timeout at ti 15.4 stack gateway

e2e.ti.com/.../597884

****************

have other advices for this ? about number of data frames in transmit queue?

i found transmit queue in Coprocessor ,to add service multi devices data request?

/* maximum number of data frames in transmit queue */

#ifndef MAC_CFG_TX_DATA_MAX
#define MAC_CFG_TX_DATA_MAX         4// 2
#endif

mac_cfg.c file

txDataMax     Maximum number of data frames queued in the transmit data queue.     1–255     2
txMax     Maximum number of frames of all types queued in the transmit data queue.     1–255     5
rxMax     Maximum number of frames queued in the receive data queue.     1–255     2
dataIndOffset     Allocate additional bytes in the data indication for application-defined headers.     0–127     0
appPendingQueue     When TRUE, registered callback of type ApiMac_pollIndFp_t will be made to the application when a data request command frame is received from another device.     TRUE or FALSE     FALSE

Thank you for considering my request.