Hi,
while using sensor controller is it possible to use any additional DIO pin other than shown in Sensor controller studio ?
In sensor controller studio, it is showing only 15 pins.
Thanks & Regards
Brijesh Varghese
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
while using sensor controller is it possible to use any additional DIO pin other than shown in Sensor controller studio ?
In sensor controller studio, it is showing only 15 pins.
Thanks & Regards
Brijesh Varghese
Hello,
no, depending on the package size, up to 15 pins can be connected to the Sensor Controller. Up to eight of these pins can be connected to analog modules.
15 for the 7x7 RGZ device,
13 for the 5x5 RHB device,
and 8 for the 4x4 RSM device.
Regards,
Andres Blanco