Tool/software: Code Composer Studio
We have bought LaunchXl-CC1310 Boards for testing
On this Boards we tested the examples from simplelink_cc13x0_sdk_1_40_00_10 .
They working fine ...
So in the meantime we have build our own rf design with an CC1310F64RHB.
But to run the examples on our custom boards are not possible, because the expamples are all for CC1310F128RGZ.
We have change the type of the µC in the propertys and we edit in the cmd file Flash size from 0x20000 to 0x10000.
Furthermore we edit the IO Definition CC1310_LAUNCHXL_SPI_FLASH_CS to an exsisting io port.
We can now start debug, but with the first rf cmd the system hangs....
So do you have any software example for the RHB Types ??
It is very hard to find out the things that must be changed....
Andreas
.