This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1350STK: Difference between CC1350STK and CC2650STK

Part Number: CC1350STK
Other Parts Discussed in Thread: CC2650STK, CC1350, CC2650

Hi,

I've been interested in sourcing  CC1350STK or CC2650STK. From the specs it looks that both are almost the same with the exception of dual-band capabilities on CC1350STK. Is CC1350STK a superset of CC2650STK in terms of features? They both are priced at 29USD. What am I missing since it looks like we can program CC1350STK for both sub-gig and 2.4GHz communication including bluetooth.