This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101: CC1101 WOR settings for lowest power consumption

Part Number: CC1101

Hello,

I'm using CC1101 in many projects, but now I need to use it in the device where I need to have a lowest current consumption in WOR mode. I've set the timers for 1800msec interval and the short duty cycle, but the problem is that it does not always wake up the receiver when I'm sending some data. I've a transmitter which transmitts 2000msec to fit for sure into one listen interval, but I need to know how to setup WOR to wake up when it detects the carrier wave (wake on based on a channel assesment) instead of preamble/key detection. I use GFSK modulation, 38.4kbps data rate. Since the duty cycle is short, then the time during the WOR activates the receiver it can detect any part of the transmitting packet which repeats in a loop continuously for 2000msec.

Michal