Tool/software: TI-RTOS
I use CC1350 REV B as keyfob 2 way on 433Mhz, with propriety protocol Manchester base.
It is base on the examples for rfPacketRx and rfPacketTx, where on the TX use patch get from TI and on the Rx use the Transparent to PIN/FIFO and low level decoding.
I am using tirtos_cc13xx_cc26xx_2_21_00_06 with IAR 7.50
The antenna is a printed one which was use already with a simple transceiver and work fine.
On the TX I get a good results but on Rx I get a very short range (about some cm!!).
Do anybody already use the CC1350 REV B as a receiver and get a good sensitivity? If so what SDK, or special setting it use?
Thanks
Bar.