This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC1310: Tx Power values less than -10 db

Part Number: CC1310


Tool/software: TI-RTOS

Hi all,

I am using 5 kbps, SimpleLink Long Range (20 kchip/s, 2-GFSK, conv. FEC r=1/2 K=7, DSSS SF=2, Tx dev.: 5 kHz, Rx BW: 49 kHz) to tranfer data. In Smartrf Studio minimum power that i can set is -10 db. But i want to set my Tx power less than this value.

I searched for Tx values but i cannot find any table or infornmation. How can i obtain all possible Tx power values that can be set? (For ex. -10 db = 0x08C0)

Best regards.

Ramazan