This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: How to improve an CollectorSensor-based use case

Expert 4031 points
Part Number: CC1310
Other Parts Discussed in Thread: CC1190

Hi,

I am using some CC1310 LaunchPads to make a demo.

The demo is based on Collector/Sensor examples running in long range mode, non-beacon. The collector will poll all the sensors every 10 sec. Data size is 512byte.

When they are in good condition (ie. LOS), the demo runs well. Error rate is just less than 1%. But when I keep them at different floors in a building, the error rate turns to higher than 30%.

I'd like to ask what are the methods to improve the situation in terms of both FW and HW.