Other Parts Discussed in Thread: CC2500
Hi,
I have design constraints on the actual size of my PCB, but not on an off-board antenna that can be fed through my PCB enclosure. Initially I had a chip antenna for the CC1310 in 915MHz mode, and was using a balun to match the CC1310 to the antenna. Unfortunately, my ground plane is not able to provide adequate enough performance for a chip antenna, and I would like to use a dipole antenna instead.
The required load impedance for the CC1310 seems to be 44 + j15. Am I able to simply design a dipole antenna with that impedance and attach it directly to the RF_N and RF_P pins, using the appropriate caps for FCC regulations as well? Or is there something else that I need to know about the CC1310's RF pins.
Thanks,