This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1110EMK868-915: Unit fails to work on HID demo

Part Number: CC1110EMK868-915
Other Parts Discussed in Thread: CC2530EMK, CC2530EM

Hi,

I want to use to the HID demo on this unit. I placed it on the smartRF05eb which recognises the emk. Programming (and verifying) the simple_hid_eb.hex file using smartRF Flash Programmer work properly, however there is no change on the unit.

I also have a CC2530emk which I can flash with its simple_hid_eb.hex and it works immediately.

What is the problem? Is it related somehow to the differences between smartRF04 and smartRF05?

Thanks,

Ariel