This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101-Q1: Question about the maximum operating temperature of the CC1101-Q1 RF Transceiver

Part Number: CC1101-Q1


Hello,

I want to use the CC1101-Q1 RF Transceiver for the development of an automotive torque sensor.

Unfortunately, the sensor requires a maximum operating temperature of 150°C but the RF Transceiver has a maximum operating temperature of 125°C due to the datasheet.

Does the transceiver also work perfectly at 150°C ?