Other Parts Discussed in Thread: CC110L,
Hello,
we are trying to integrate a device using the CC1310 transceiver into an existing ecosystem of devices using different transceivers. Most of these devices use a data rate of 20.4kBaud, but some use 20.8kBaud. Compatibility has not been an issue before, since the transceivers used offered the ability to compensate for data rate offset. For example: one of the transceivers used in our system is the CC110L, it offers programmable data rate offset tolerance of up to 3.125% (BS_LIMIT[1:0]).
The CC1310 however seems to have a fixed data rate offset tolerance of typically 1600ppm. Is there an override or a patch to change this? We require higher tolerance to make the CC1310 work in our system. We can not change the data rate of other devices since they are already deployed.
Best regards