I've been developing a device for the Internet of Things on the basis of TI CC1310 chip. Designed software runs OK on TI debug boards - the connection is established, the data is exchanged without any loss.
But when I upload my firmware to the custom designed circuit board I see connection established but no data passed through. Thus, if I connect the circuits using SmartRF Studio from TI and debug boards they are fully functional: RSSI and the number of errors the same as in debug boards. I've checked the transceiver function through the antennas on the circuits, copied from debug board, and by a coaxial cable - the result is identical.