This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: PG 2.0 vs. PG 2.1

Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310

Hi team,

We were using the PG 2.0 CC1310 LaunchPad and now have the PG 2.1 CC1310 LaunchPad. We are running the same firmware on the two platforms but in our testing we are having our PG 2.1 board run into error and TX/RX stops in less than 6 hours. However, we were not having any issues when running the same test on our PG 2.0 board.

What are the differences in the silicon PG 2.0 vs. PG 2.1? Are there any register settings that we need to change between the two or an SDK incompatibility?

Regards,

Akash Patel