Tool/software: Code Composer Studio
Hi,
Because I have 2 transmitters which transmit the packet at different frequency (431 MHz and 432 MHz), could I receive their packets via only one board? For instance, could I change the received frequency periodically of Rx? I attempt to modify the code examples in CCS, "rfPacketRx.c" and "smartrf_settings.c" .
Here is the time slot of the receiver.
Thank you!
Best regards,