Other Parts Discussed in Thread: CC1310
Hi,
I've 2 CC1310 Launchpad boards. If I configure them to work with 915MHz then everything is ok, they work. But if I configure them for 868MHz things change and the boards seems to be not stable at all. If I lift or hold in a specific way they for a while they seem to work but then the connection is lost again. From this I understand that the antenna on PCB is optimized for 915MHz right? Is there a predefined way to convert or adapt it for 868MHz working?
Thanks in advance...