Other Parts Discussed in Thread: CC1350, CC1310
I am looking at using a cc1350 launchpad to talk to an existing receiver for a homebrew project of mine.
The receiver is configured:
- 433.92 MHz center frequency
- FSK modulation
- FSK peak deviation of 30 kHz
- Preamble = 16 bits
- Sync word = 13 bits
- Data = 16 bits
- Bits are Manchester-encoded before being transmitted
- 1.2 kbits/sec data rate
I've looked over the reference manual and I am not sure if those preamble, sync word, and data lengths will work.
Also, I read that the cc1350 doesn't do Manchester encoding on the sync word?
Is the cc1350 capable of transmitting according to these requirements?
Thanks
Alex