Tool/software: Code Composer Studio
I'm using the example 'RfWsnDmConcentrator' for CC1350 Launchpad. As a node (normally RfWsnDmConcentrator with an other CC1350), i would use a CC1101. I have a the EZ430 RF Access Point (White Board, MSP430F5509 + CC1101) with the corresponding USB-Emulator for debugging.
Is it possible to transmit data from the node (TX, Access point) to the concentrator (RX, CC1350)? Should I try to use EasyLink on the Access Point?
I identified all the RF parameters of the example 'RfWsnDmConcentrator' from SmartRF Studio, but SmartRF Studio doens't support the EZ430 hardware.
I need suggestions which protocols or software i can use for this task.
Thank you