Other Parts Discussed in Thread: TPD1E0B04
Hi,
i have a big problem since 1 year. We use CC1120 in our outdoor products, whereby we transmit data from sensor nodes to main station. We had many cases, when all nodes were lost at once. The problem appeared on main station apparently. After investigations we found this followed issue:
- The signal from the main station is hardly to catch and if we have signal, only very poor -110 to -120 dBm (only if we are 1-2 meter far from main station)
- The signal from sensor node at main station is very good (I suppose, the receiver is working well).
- cc1120 is heating up during TX transmitting and current goes up to about 170 mA.
After that I found this curiosity: The resistance between PA and Ground is only 8 - 9 Ohm. Uff. Normally i would expected High-Z or very high resistance. I compared it with new CC1120 module, and really the new one has about 2 MOhm on PA to Ground. That is the reason of high current consumption during tx mode and too low output performance. LNA_P and LNA_N inputs seem to be ok.
Has anybody met such similar issue? The only solution for this issue we had, was main station changing. After we had much more problems we have investigated in last time and found this problem. If it would help you, i can provide my schematic using CC1120 and layouts of th board.
The question is, what happened, what could cause this issue?
Thanks
Best regards,
Jan