Other Parts Discussed in Thread: CC1125, CC1310, CC1200, CC1190,
Hello,
Is there a simple comparison chart between CC1310 & CC1312? I haven't heard much about the radio - is it the same between them or does the CC1312 have better performance for narrowband applications (like CC1125, CC1200)?
Also, is there an AT-command interface Network Processor firmware for the CC1312, like you had for the CC1310? (see this link)
Finally, will the CC1312 be easier to connect to the CC1190 (or other PA/LNA)? The CC1310+CC1190 design was a mess.
Thanks,
Derek