Here is part of my code, I can't still get the bit stream of CC1310's RF, is something wrong?
smartrf_settings.c:
```
static uint32_t pOverrides[] = {
// Set the SYSGPOCTL register
HW_REG_OVERRIDE(0x1110, (4 | 5 << 4)), // MCE0 -> RFC_GPO0, MCE1 -> RFC_GPO1
...
}
```
mainThread.c
```
...
PIN_Handle pinHandle;
PIN_State pinstate;
PIN_Config pinTable[] = {
IOID_21 | PIN_GPIO_OUTPUT_EN | PIN_PUSHPULL | PIN_DRVSTR_MAX | PIN_GPIO_LOW,
IOID_22 | PIN_GPIO_OUTPUT_EN | PIN_PUSHPULL | PIN_DRVSTR_MAX | PIN_GPIO_LOW,
PIN_TERMINATE
};
/** Functions */
void foo3(void) {
pinHandle = PIN_open(&pinstate, pinTable);
/** Init Rf */
RF_Object rf_object;
RF_Params rf_params;
RF_Params_init(&rf_params);
rf_handle_g = RF_open(&rf_object, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rf_params); /* Request access to the radio */
RF_cmdFs.synthConf.bTxMode = 1;
RF_runCmd(rf_handle_g, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0); /* Set the frequency */
int i = CC1310_RFC_DBELL.SYSGPOCTL; // This value is 0x54, which means MCE0 -> RFC_GPO0, MCE1 -> RFC_GPO1
// Map RFC_GPO0 to IO 21
PINCC26XX_setMux(pinHandle, IOID_21, PINCC26XX_MUX_RFC_GPO0);
/// Map RFC_GPO1 to IO 22
PINCC26XX_setMux(pinHandle, IOID_22, PINCC26XX_MUX_RFC_GPO1);
/** Main procedure */
CmdPropTx(rf_handle_g);
}
...
```