This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1350: Wide-Band DSSS and FEC

Part Number: CC1350


Hello all,

Below is smart rf settings which i am using to incorporate the DSSS......I am operating at 58 kbps with 4 bit preamble, 14 bit syncword and 8 bit crc.

I replaced this setting with the setting given in packet tx example project.

HW_REG_OVERRIDE(0x52AC, 0x073C), ........implies the x8 spreading factor.  so total number of bits are 1946 (4+14+8 for crc+30*8*8). At 58 kbps packet duration is  75.4 ms. But it should be 1946/58 = 33.51 ms. Please once check my settings specially override part. And why it is giving more timeperiod.

HW_REG_OVERRIDE(0x52AC, 0x073C),

//*********************************************************************************
// Generated by SmartRF Studio version 2.6.0 (build #8)
// Tested for SimpleLink SDK version: CC13x0 SDK 1.30.xx.xx
// Device: CC1350 Rev. 2.1 (Rev. B)
//
//*********************************************************************************
 
 
//*********************************************************************************
// Parameter summary
// Address: off
// Address0: 0xAA
// Address1: 0xBB
// Frequency: 433.92000 MHz
// Data Format: Serial mode disable
// Deviation: 25.000 kHz
// Packet Length Config: Variable
// Max Packet Length: 128
// Packet Length: 20
// RX Filter BW: 98 kHz
// Symbol Rate: 50.00000 kBaud
// Sync Word Length: 32 Bits
// TX Power: 15 dBm (requires define CCFG_FORCE_VDDR_HH = 1 in ccfg.c, see CC13xx/CC26xx Technical Reference Manual)
// Whitening: No whitening
 
 
#include <ti/devices/DeviceFamily.h>
#include DeviceFamily_constructPath(driverlib/rf_mailbox.h)
#include DeviceFamily_constructPath(driverlib/rf_common_cmd.h)
#include DeviceFamily_constructPath(driverlib/rf_prop_cmd.h)
#include <ti/drivers/rf/RF.h>
#include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_genfsk.h)
#include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_genfsk.h)
 
 
#include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_wb_dsss.h)    //added by me
#include DeviceFamily_constructPath(rf_patches/rf_patch_mce_wb_dsss.h)    //added by me
#include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_wb_dsss.h)    //added by me
 
 
#include "smartrf_settings.h"
 
 
// TI-RTOS RF Mode Object
RF_Mode RF_prop =
{
    .rfMode = RF_MODE_PROPRIETARY_SUB_1,
   // .cpePatchFxn = &rf_patch_cpe_genfsk,
    .cpePatchFxn = &rf_patch_cpe_wb_dsss,   //added by me
  //  .mcePatchFxn = 0,
    .mcePatchFxn = &rf_patch_mce_wb_dsss,   //added by me
  //  .rfePatchFxn = &rf_patch_rfe_genfsk,
    .rfePatchFxn = &rf_patch_rfe_wb_dsss,   //added by me
};
 
// Overrides for CMD_PROP_RADIO_DIV_SETUP
static uint32_t pOverrides[] =
{
  //   override_use_patch_prop_genfsk.xml
    // PHY: Use MCE ROM bank 4, RFE RAM patch
  //   MCE_RFE_OVERRIDE(0,4,0,1,0,0),
     MCE_RFE_OVERRIDE(1,0,0,1,0,0),     //added by me
    // override_synth_prop_430_510_div10.xml
    // Synth: Set recommended RTRIM to 7
    HW_REG_OVERRIDE(0x4038,0x0037),
    // Synth: Set Fref to 4 MHz
    (uint32_t)0x000684A3,
    // Synth: Configure fine calibration setting
    HW_REG_OVERRIDE(0x4020,0x7F00),
    // Synth: Configure fine calibration setting
    HW_REG_OVERRIDE(0x4064,0x0040),
    // Synth: Configure fine calibration setting
    (uint32_t)0xB1070503,
    // Synth: Configure fine calibration setting
    (uint32_t)0x05330523,
    // Synth: Set loop bandwidth after lock to 20 kHz
    (uint32_t)0x0A480583,
    // Synth: Set loop bandwidth after lock to 20 kHz
    (uint32_t)0x7AB80603,
    // Synth: Configure VCO LDO (in ADI1, set VCOLDOCFG=0x9F to use voltage input reference)
    ADI_REG_OVERRIDE(1,4,0x9F),
    // Synth: Configure synth LDO (in ADI1, set SLDOCTL0.COMP_CAP=1)
    ADI_HALFREG_OVERRIDE(1,7,0x4,0x4),
    // Synth: Use 24 MHz XOSC as synth clock, enable extra PLL filtering
    (uint32_t)0x02010403,
    // Synth: Configure extra PLL filtering
    (uint32_t)0x00108463,
    // Synth: Increase synth programming timeout (0x04B0 RAT ticks = 300 us)
    (uint32_t)0x04B00243,
    // override_synth_disable_bias_div10.xml
    // Synth: Set divider bias to disabled
    HW32_ARRAY_OVERRIDE(0x405C,1),
    // Synth: Set divider bias to disabled (specific for loDivider=10)
    (uint32_t)0x18000280,
    // override_phy_rx_aaf_bw_0xd.xml
    // Rx: Set anti-aliasing filter bandwidth to 0xD (in ADI0, set IFAMPCTL3[7:4]=0xD)
    ADI_HALFREG_OVERRIDE(0,61,0xF,0xD),
    // override_phy_gfsk_rx.xml
    // Rx: Set LNA bias current trim offset to 3
    (uint32_t)0x00038883,
    // Rx: Freeze RSSI on sync found event
    HW_REG_OVERRIDE(0x6084,0x35F1),
    // override_phy_gfsk_pa_ramp_agc_reflevel_0x1a.xml
    // Tx: Configure PA ramping setting (0x41). Rx: Set AGC reference level to 0x1A.
 //   HW_REG_OVERRIDE(0x6088,0x411A),
 //   HW_REG_OVERRIDE(0x6088,0x410E),      //added by me   AGC REFRENCE LEVEL
      HW_REG_OVERRIDE(0x6088,0x1F0E),      //added by me   AGC REFRENCE LEVEL
    // Tx: Configure PA ramping setting
 //   HW_REG_OVERRIDE(0x608C,0x8213),
      HW_REG_OVERRIDE(0x608C,0x3F13),      //added by me
      HW_REG_OVERRIDE(0x52AC, 0x073C),   //added by me  DSSS = 4, K = 4 DATA RATE 62.5 kbps
   //   HW_REG_OVERRIDE(0x505C, 0x0303),     //added by me    DSSS = 8
      HW_REG_OVERRIDE(0x5108, 0x0048),     // added by me correlator sync threshold
    // override_phy_rx_rssi_offset_neg2db.xml
    // Rx: Set RSSI offset to adjust reported RSSI by -2 dB
    (uint32_t)0x00FB88A3,
    (uint32_t)0x000288A3,
    // TX power override
    // Tx: Set PA trim to max (in ADI0, set PACTL0=0xF8)
    ADI_REG_OVERRIDE(0,12,0xF8),
    (uint32_t)0xFFFFFFFF,
};
 
 
// CMD_PROP_RADIO_DIV_SETUP
// Proprietary Mode Radio Setup Command for All Frequency Bands
rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup =
{
    .commandNo = 0x3807,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .modulation.modType = 0x1,
    .modulation.deviation = 0x64,
    .symbolRate.preScale = 0xF,
    .symbolRate.rateWord = 0x947B,
    .rxBw = 0x24,
    .preamConf.nPreamBytes = 0x1F,
    .preamConf.preamMode = 0x0,
    .formatConf.nSwBits = 0xE,
    .formatConf.bBitReversal = 0x0,
    .formatConf.bMsbFirst = 0x1,
    .formatConf.fecMode = 0x0,
    .formatConf.whitenMode = 0x0,
    .config.frontEndMode = 0x0,
    .config.biasMode = 0x1,
    .config.analogCfgMode = 0x0,
    .config.bNoFsPowerUp = 0x0,
    .txPower = 0x003F,
    .pRegOverride = pOverrides,
    .centerFreq = 0x01BB,
    .intFreq = 0x8000,
    .loDivider = 0x0A,
};
 
// CMD_FS
// Frequency Synthesizer Programming Command
rfc_CMD_FS_t RF_cmdFs =
{
    .commandNo = 0x0803,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx  Pointer to the next operation to run after this operation is done
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0, //*********************************************************************************
// Generated by SmartRF Studio version 2.6.0 (build #8)
// Tested for SimpleLink SDK version: CC13x0 SDK 1.30.xx.xx
// Device: CC1350 Rev. 2.1 (Rev. B)
//
//*********************************************************************************
 
 
//*********************************************************************************
// Parameter summary
// Address: off
// Address0: 0xAA
// Address1: 0xBB
// Frequency: 433.92000 MHz
// Data Format: Serial mode disable
// Deviation: 25.000 kHz
// Packet Length Config: Variable
// Max Packet Length: 128
// Packet Length: 20
// RX Filter BW: 98 kHz
// Symbol Rate: 50.00000 kBaud
// Sync Word Length: 32 Bits
// TX Power: 15 dBm (requires define CCFG_FORCE_VDDR_HH = 1 in ccfg.c, see CC13xx/CC26xx Technical Reference Manual)
// Whitening: No whitening
 
 
#include <ti/devices/DeviceFamily.h>
#include DeviceFamily_constructPath(driverlib/rf_mailbox.h)
#include DeviceFamily_constructPath(driverlib/rf_common_cmd.h)
#include DeviceFamily_constructPath(driverlib/rf_prop_cmd.h)
#include <ti/drivers/rf/RF.h>
#include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_genfsk.h)
#include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_genfsk.h)
 
 
#include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_wb_dsss.h)    //added by me
#include DeviceFamily_constructPath(rf_patches/rf_patch_mce_wb_dsss.h)    //added by me
#include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_wb_dsss.h)    //added by me
 
 
#include "smartrf_settings.h"
 
 
// TI-RTOS RF Mode Object
RF_Mode RF_prop =
{
    .rfMode = RF_MODE_PROPRIETARY_SUB_1,
   // .cpePatchFxn = &rf_patch_cpe_genfsk,
    .cpePatchFxn = &rf_patch_cpe_wb_dsss,   //added by me
  //  .mcePatchFxn = 0,
    .mcePatchFxn = &rf_patch_mce_wb_dsss,   //added by me
  //  .rfePatchFxn = &rf_patch_rfe_genfsk,
    .rfePatchFxn = &rf_patch_rfe_wb_dsss,   //added by me
};
 
// Overrides for CMD_PROP_RADIO_DIV_SETUP
static uint32_t pOverrides[] =
{
  //   override_use_patch_prop_genfsk.xml
    // PHY: Use MCE ROM bank 4, RFE RAM patch
  //   MCE_RFE_OVERRIDE(0,4,0,1,0,0),
     MCE_RFE_OVERRIDE(1,0,0,1,0,0),     //added by me
    // override_synth_prop_430_510_div10.xml
    // Synth: Set recommended RTRIM to 7
    HW_REG_OVERRIDE(0x4038,0x0037),
    // Synth: Set Fref to 4 MHz
    (uint32_t)0x000684A3,
    // Synth: Configure fine calibration setting
    HW_REG_OVERRIDE(0x4020,0x7F00),
    // Synth: Configure fine calibration setting
    HW_REG_OVERRIDE(0x4064,0x0040),
    // Synth: Configure fine calibration setting
    (uint32_t)0xB1070503,
    // Synth: Configure fine calibration setting
    (uint32_t)0x05330523,
    // Synth: Set loop bandwidth after lock to 20 kHz
    (uint32_t)0x0A480583,
    // Synth: Set loop bandwidth after lock to 20 kHz
    (uint32_t)0x7AB80603,
    // Synth: Configure VCO LDO (in ADI1, set VCOLDOCFG=0x9F to use voltage input reference)
    ADI_REG_OVERRIDE(1,4,0x9F),
    // Synth: Configure synth LDO (in ADI1, set SLDOCTL0.COMP_CAP=1)
    ADI_HALFREG_OVERRIDE(1,7,0x4,0x4),
    // Synth: Use 24 MHz XOSC as synth clock, enable extra PLL filtering
    (uint32_t)0x02010403,
    // Synth: Configure extra PLL filtering
    (uint32_t)0x00108463,
    // Synth: Increase synth programming timeout (0x04B0 RAT ticks = 300 us)
    (uint32_t)0x04B00243,
    // override_synth_disable_bias_div10.xml
    // Synth: Set divider bias to disabled
    HW32_ARRAY_OVERRIDE(0x405C,1),
    // Synth: Set divider bias to disabled (specific for loDivider=10)
    (uint32_t)0x18000280,
    // override_phy_rx_aaf_bw_0xd.xml
    // Rx: Set anti-aliasing filter bandwidth to 0xD (in ADI0, set IFAMPCTL3[7:4]=0xD)
    ADI_HALFREG_OVERRIDE(0,61,0xF,0xD),
    // override_phy_gfsk_rx.xml
    // Rx: Set LNA bias current trim offset to 3
    (uint32_t)0x00038883,
    // Rx: Freeze RSSI on sync found event
    HW_REG_OVERRIDE(0x6084,0x35F1),
    // override_phy_gfsk_pa_ramp_agc_reflevel_0x1a.xml
    // Tx: Configure PA ramping setting (0x41). Rx: Set AGC reference level to 0x1A.
 //   HW_REG_OVERRIDE(0x6088,0x411A),
 //   HW_REG_OVERRIDE(0x6088,0x410E),      //added by me   AGC REFRENCE LEVEL
      HW_REG_OVERRIDE(0x6088,0x1F0E),      //added by me   AGC REFRENCE LEVEL
    // Tx: Configure PA ramping setting
 //   HW_REG_OVERRIDE(0x608C,0x8213),
      HW_REG_OVERRIDE(0x608C,0x3F13),      //added by me
      HW_REG_OVERRIDE(0x52AC, 0x073C),   //added by me  DSSS = 4, K = 4 DATA RATE 62.5 kbps
   //   HW_REG_OVERRIDE(0x505C, 0x0303),     //added by me    DSSS = 8
      HW_REG_OVERRIDE(0x5108, 0x0048),     // added by me correlator sync threshold
    // override_phy_rx_rssi_offset_neg2db.xml
    // Rx: Set RSSI offset to adjust reported RSSI by -2 dB
    (uint32_t)0x00FB88A3,
    (uint32_t)0x000288A3,
    // TX power override
    // Tx: Set PA trim to max (in ADI0, set PACTL0=0xF8)
    ADI_REG_OVERRIDE(0,12,0xF8),
    (uint32_t)0xFFFFFFFF,
};
 
 
// CMD_PROP_RADIO_DIV_SETUP
// Proprietary Mode Radio Setup Command for All Frequency Bands
rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup =
{
    .commandNo = 0x3807,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .modulation.modType = 0x1,
    .modulation.deviation = 0x64,
    .symbolRate.preScale = 0xF,
    .symbolRate.rateWord = 0x947B,
    .rxBw = 0x24,
    .preamConf.nPreamBytes = 0x1F,
    .preamConf.preamMode = 0x0,
    .formatConf.nSwBits = 0xE,
    .formatConf.bBitReversal = 0x0,
    .formatConf.bMsbFirst = 0x1,
    .formatConf.fecMode = 0x0,
    .formatConf.whitenMode = 0x0,
    .config.frontEndMode = 0x0,
    .config.biasMode = 0x1,
    .config.analogCfgMode = 0x0,
    .config.bNoFsPowerUp = 0x0,
    .txPower = 0x003F,
    .pRegOverride = pOverrides,
    .centerFreq = 0x01BB,
    .intFreq = 0x8000,
    .loDivider = 0x0A,
};
 
// CMD_FS
// Frequency Synthesizer Programming Command
rfc_CMD_FS_t RF_cmdFs =
{
    .commandNo = 0x0803,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx  Pointer to the next operation to run after this operation is done
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .frequency = 0x01BB,
    .fractFreq = 0xEB85,
    .synthConf.bTxMode = 0x0,
    .synthConf.refFreq = 0x0,
    .__dummy0 = 0x00,
    .__dummy1 = 0x00,
    .__dummy2 = 0x00,
    .__dummy3 = 0x0000,
};
 
// CMD_PROP_TX
// Proprietary Mode Transmit Command
rfc_CMD_PROP_TX_t RF_cmdPropTx =
{
    .commandNo = 0x3801,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .pktConf.bFsOff = 0x0,
    .pktConf.bUseCrc = 0x1,
    .pktConf.bVarLen = 0x1,
    .pktLen = 0x14, // SET APPLICATION PAYLOAD LENGTH
    .syncWord = 0x930B51DE,
    .pPkt = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};
 
// CMD_PROP_RX
// Proprietary Mode Receive Command
rfc_CMD_PROP_RX_t RF_cmdPropRx =
{
    .commandNo = 0x3802,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .pktConf.bFsOff = 0x0,
    .pktConf.bRepeatOk = 0x0,
    .pktConf.bRepeatNok = 0x0,
    .pktConf.bUseCrc = 0x1,
    .pktConf.bVarLen = 0x1,
    .pktConf.bChkAddress = 0x0,
    .pktConf.endType = 0x0,
    .pktConf.filterOp = 0x0,
    .rxConf.bAutoFlushIgnored = 0x0,
    .rxConf.bAutoFlushCrcErr = 0x0,
    .rxConf.bIncludeHdr = 0x1,
    .rxConf.bIncludeCrc = 0x0,
    .rxConf.bAppendRssi = 0x0,
    .rxConf.bAppendTimestamp = 0x0,
    .rxConf.bAppendStatus = 0x1,
    .syncWord = 0x930B51DE,
    .maxPktLen = 0x80, // MAKE SURE DATA ENTRY IS LARGE ENOUGH
    .address0 = 0xAA,
    .address1 = 0xBB,
    .endTrigger.triggerType = 0x1,
    .endTrigger.bEnaCmd = 0x0,
    .endTrigger.triggerNo = 0x0,
    .endTrigger.pastTrig = 0x0,
    .endTime = 0x00000000,
    .pQueue = 0, // INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx
    .pOutput = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};
 
// CMD_TX_TEST
// Transmitter Test Command
rfc_CMD_TX_TEST_t RF_cmdTxTest =
{
    .commandNo = 0x0808,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .config.bUseCw = 0x0,
    .config.bFsOff = 0x1,
    .config.whitenMode = 0x2,
    .__dummy0 = 0x00,
    .txWord = 0xABCD,
    .__dummy1 = 0x00,
    .endTrigger.triggerType = 0x1,
    .endTrigger.bEnaCmd = 0x0,
    .endTrigger.triggerNo = 0x0,
    .endTrigger.pastTrig = 0x0,
    .syncWord = 0x930B51DE,
    .endTime = 0x00000000,
};
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .frequency = 0x01BB,
    .fractFreq = 0xEB85,
    .synthConf.bTxMode = 0x0,
    .synthConf.refFreq = 0x0,
    .__dummy0 = 0x00,
    .__dummy1 = 0x00,
    .__dummy2 = 0x00,
    .__dummy3 = 0x0000,
};
 
// CMD_PROP_TX
// Proprietary Mode Transmit Command
rfc_CMD_PROP_TX_t RF_cmdPropTx =
{
    .commandNo = 0x3801,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .pktConf.bFsOff = 0x0,
    .pktConf.bUseCrc = 0x1,
    .pktConf.bVarLen = 0x1,
    .pktLen = 0x14, // SET APPLICATION PAYLOAD LENGTH
    .syncWord = 0x930B51DE,
    .pPkt = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};
 
// CMD_PROP_RX
// Proprietary Mode Receive Command
rfc_CMD_PROP_RX_t RF_cmdPropRx =
{
    .commandNo = 0x3802,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .pktConf.bFsOff = 0x0,
    .pktConf.bRepeatOk = 0x0,
    .pktConf.bRepeatNok = 0x0,
    .pktConf.bUseCrc = 0x1,
    .pktConf.bVarLen = 0x1,
    .pktConf.bChkAddress = 0x0,
    .pktConf.endType = 0x0,
    .pktConf.filterOp = 0x0,
    .rxConf.bAutoFlushIgnored = 0x0,
    .rxConf.bAutoFlushCrcErr = 0x0,
    .rxConf.bIncludeHdr = 0x1,
    .rxConf.bIncludeCrc = 0x0,
    .rxConf.bAppendRssi = 0x0,
    .rxConf.bAppendTimestamp = 0x0,
    .rxConf.bAppendStatus = 0x1,
    .syncWord = 0x930B51DE,
    .maxPktLen = 0x80, // MAKE SURE DATA ENTRY IS LARGE ENOUGH
    .address0 = 0xAA,
    .address1 = 0xBB,
    .endTrigger.triggerType = 0x1,
    .endTrigger.bEnaCmd = 0x0,
    .endTrigger.triggerNo = 0x0,
    .endTrigger.pastTrig = 0x0,
    .endTime = 0x00000000,
    .pQueue = 0, // INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx
    .pOutput = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};
 
// CMD_TX_TEST
// Transmitter Test Command
rfc_CMD_TX_TEST_t RF_cmdTxTest =
{
    .commandNo = 0x0808,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .config.bUseCw = 0x0,
    .config.bFsOff = 0x1,
    .config.whitenMode = 0x2,
    .__dummy0 = 0x00,
    .txWord = 0xABCD,
    .__dummy1 = 0x00,
    .endTrigger.triggerType = 0x1,
    .endTrigger.bEnaCmd = 0x0,
    .endTrigger.triggerNo = 0x0,
    .endTrigger.pastTrig = 0x0,
    .syncWord = 0x930B51DE,
    .endTime = 0x00000000,
};//*********************************************************************************
// Generated by SmartRF Studio version 2.6.0 (build #8)
// Tested for SimpleLink SDK version: CC13x0 SDK 1.30.xx.xx
// Device: CC1350 Rev. 2.1 (Rev. B)
//
//*********************************************************************************
 
 
//*********************************************************************************
// Parameter summary
// Address: off
// Address0: 0xAA
// Address1: 0xBB
// Frequency: 433.92000 MHz
// Data Format: Serial mode disable
// Deviation: 25.000 kHz
// Packet Length Config: Variable
// Max Packet Length: 128
// Packet Length: 20
// RX Filter BW: 98 kHz
// Symbol Rate: 50.00000 kBaud
// Sync Word Length: 32 Bits
// TX Power: 15 dBm (requires define CCFG_FORCE_VDDR_HH = 1 in ccfg.c, see CC13xx/CC26xx Technical Reference Manual)
// Whitening: No whitening
 
 
#include <ti/devices/DeviceFamily.h>
#include DeviceFamily_constructPath(driverlib/rf_mailbox.h)
#include DeviceFamily_constructPath(driverlib/rf_common_cmd.h)
#include DeviceFamily_constructPath(driverlib/rf_prop_cmd.h)
#include <ti/drivers/rf/RF.h>
#include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_genfsk.h)
#include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_genfsk.h)
 
 
#include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_wb_dsss.h)    //added by me
#include DeviceFamily_constructPath(rf_patches/rf_patch_mce_wb_dsss.h)    //added by me
#include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_wb_dsss.h)    //added by me
 
 
#include "smartrf_settings.h"
 
 
// TI-RTOS RF Mode Object
RF_Mode RF_prop =
{
    .rfMode = RF_MODE_PROPRIETARY_SUB_1,
   // .cpePatchFxn = &rf_patch_cpe_genfsk,
    .cpePatchFxn = &rf_patch_cpe_wb_dsss,   //added by me
  //  .mcePatchFxn = 0,
    .mcePatchFxn = &rf_patch_mce_wb_dsss,   //added by me
  //  .rfePatchFxn = &rf_patch_rfe_genfsk,
    .rfePatchFxn = &rf_patch_rfe_wb_dsss,   //added by me
};
 
// Overrides for CMD_PROP_RADIO_DIV_SETUP
static uint32_t pOverrides[] =
{
  //   override_use_patch_prop_genfsk.xml
    // PHY: Use MCE ROM bank 4, RFE RAM patch
  //   MCE_RFE_OVERRIDE(0,4,0,1,0,0),
     MCE_RFE_OVERRIDE(1,0,0,1,0,0),     //added by me
    // override_synth_prop_430_510_div10.xml
    // Synth: Set recommended RTRIM to 7
    HW_REG_OVERRIDE(0x4038,0x0037),
    // Synth: Set Fref to 4 MHz
    (uint32_t)0x000684A3,
    // Synth: Configure fine calibration setting
    HW_REG_OVERRIDE(0x4020,0x7F00),
    // Synth: Configure fine calibration setting
    HW_REG_OVERRIDE(0x4064,0x0040),
    // Synth: Configure fine calibration setting
    (uint32_t)0xB1070503,
    // Synth: Configure fine calibration setting
    (uint32_t)0x05330523,
    // Synth: Set loop bandwidth after lock to 20 kHz
    (uint32_t)0x0A480583,
    // Synth: Set loop bandwidth after lock to 20 kHz
    (uint32_t)0x7AB80603,
    // Synth: Configure VCO LDO (in ADI1, set VCOLDOCFG=0x9F to use voltage input reference)
    ADI_REG_OVERRIDE(1,4,0x9F),
    // Synth: Configure synth LDO (in ADI1, set SLDOCTL0.COMP_CAP=1)
    ADI_HALFREG_OVERRIDE(1,7,0x4,0x4),
    // Synth: Use 24 MHz XOSC as synth clock, enable extra PLL filtering
    (uint32_t)0x02010403,
    // Synth: Configure extra PLL filtering
    (uint32_t)0x00108463,
    // Synth: Increase synth programming timeout (0x04B0 RAT ticks = 300 us)
    (uint32_t)0x04B00243,
    // override_synth_disable_bias_div10.xml
    // Synth: Set divider bias to disabled
    HW32_ARRAY_OVERRIDE(0x405C,1),
    // Synth: Set divider bias to disabled (specific for loDivider=10)
    (uint32_t)0x18000280,
    // override_phy_rx_aaf_bw_0xd.xml
    // Rx: Set anti-aliasing filter bandwidth to 0xD (in ADI0, set IFAMPCTL3[7:4]=0xD)
    ADI_HALFREG_OVERRIDE(0,61,0xF,0xD),
    // override_phy_gfsk_rx.xml
    // Rx: Set LNA bias current trim offset to 3
    (uint32_t)0x00038883,
    // Rx: Freeze RSSI on sync found event
    HW_REG_OVERRIDE(0x6084,0x35F1),
    // override_phy_gfsk_pa_ramp_agc_reflevel_0x1a.xml
    // Tx: Configure PA ramping setting (0x41). Rx: Set AGC reference level to 0x1A.
 //   HW_REG_OVERRIDE(0x6088,0x411A),
 //   HW_REG_OVERRIDE(0x6088,0x410E),      //added by me   AGC REFRENCE LEVEL
      HW_REG_OVERRIDE(0x6088,0x1F0E),      //added by me   AGC REFRENCE LEVEL
    // Tx: Configure PA ramping setting
 //   HW_REG_OVERRIDE(0x608C,0x8213),
      HW_REG_OVERRIDE(0x608C,0x3F13),      //added by me
      HW_REG_OVERRIDE(0x52AC, 0x073C),   //added by me  DSSS = 4, K = 4 DATA RATE 62.5 kbps
   //   HW_REG_OVERRIDE(0x505C, 0x0303),     //added by me    DSSS = 8
      HW_REG_OVERRIDE(0x5108, 0x0048),     // added by me correlator sync threshold
    // override_phy_rx_rssi_offset_neg2db.xml
    // Rx: Set RSSI offset to adjust reported RSSI by -2 dB
    (uint32_t)0x00FB88A3,
    (uint32_t)0x000288A3,
    // TX power override
    // Tx: Set PA trim to max (in ADI0, set PACTL0=0xF8)
    ADI_REG_OVERRIDE(0,12,0xF8),
    (uint32_t)0xFFFFFFFF,
};
 
 
// CMD_PROP_RADIO_DIV_SETUP
// Proprietary Mode Radio Setup Command for All Frequency Bands
rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup =
{
    .commandNo = 0x3807,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .modulation.modType = 0x1,
    .modulation.deviation = 0x64,
    .symbolRate.preScale = 0xF,
    .symbolRate.rateWord = 0x947B,
    .rxBw = 0x24,
    .preamConf.nPreamBytes = 0x1F,
    .preamConf.preamMode = 0x0,
    .formatConf.nSwBits = 0xE,
    .formatConf.bBitReversal = 0x0,
    .formatConf.bMsbFirst = 0x1,
    .formatConf.fecMode = 0x0,
    .formatConf.whitenMode = 0x0,
    .config.frontEndMode = 0x0,
    .config.biasMode = 0x1,
    .config.analogCfgMode = 0x0,
    .config.bNoFsPowerUp = 0x0,
    .txPower = 0x003F,
    .pRegOverride = pOverrides,
    .centerFreq = 0x01BB,
    .intFreq = 0x8000,
    .loDivider = 0x0A,
};
 
// CMD_FS
// Frequency Synthesizer Programming Command
rfc_CMD_FS_t RF_cmdFs =
{
    .commandNo = 0x0803,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx  Pointer to the next operation to run after this operation is done
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .frequency = 0x01BB,
    .fractFreq = 0xEB85,
    .synthConf.bTxMode = 0x0,
    .synthConf.refFreq = 0x0,
    .__dummy0 = 0x00,
    .__dummy1 = 0x00,
    .__dummy2 = 0x00,
    .__dummy3 = 0x0000,
};
 
// CMD_PROP_TX
// Proprietary Mode Transmit Command
rfc_CMD_PROP_TX_t RF_cmdPropTx =
{
    .commandNo = 0x3801,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .pktConf.bFsOff = 0x0,
    .pktConf.bUseCrc = 0x1,
    .pktConf.bVarLen = 0x1,
    .pktLen = 0x14, // SET APPLICATION PAYLOAD LENGTH
    .syncWord = 0x930B51DE,
    .pPkt = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};
 
// CMD_PROP_RX
// Proprietary Mode Receive Command
rfc_CMD_PROP_RX_t RF_cmdPropRx =
{
    .commandNo = 0x3802,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .pktConf.bFsOff = 0x0,
    .pktConf.bRepeatOk = 0x0,
    .pktConf.bRepeatNok = 0x0,
    .pktConf.bUseCrc = 0x1,
    .pktConf.bVarLen = 0x1,
    .pktConf.bChkAddress = 0x0,
    .pktConf.endType = 0x0,
    .pktConf.filterOp = 0x0,
    .rxConf.bAutoFlushIgnored = 0x0,
    .rxConf.bAutoFlushCrcErr = 0x0,
    .rxConf.bIncludeHdr = 0x1,
    .rxConf.bIncludeCrc = 0x0,
    .rxConf.bAppendRssi = 0x0,
    .rxConf.bAppendTimestamp = 0x0,
    .rxConf.bAppendStatus = 0x1,
    .syncWord = 0x930B51DE,
    .maxPktLen = 0x80, // MAKE SURE DATA ENTRY IS LARGE ENOUGH
    .address0 = 0xAA,
    .address1 = 0xBB,
    .endTrigger.triggerType = 0x1,
    .endTrigger.bEnaCmd = 0x0,
    .endTrigger.triggerNo = 0x0,
    .endTrigger.pastTrig = 0x0,
    .endTime = 0x00000000,
    .pQueue = 0, // INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx
    .pOutput = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};
 
// CMD_TX_TEST
// Transmitter Test Command
rfc_CMD_TX_TEST_t RF_cmdTxTest =
{
    .commandNo = 0x0808,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .config.bUseCw = 0x0,
    .config.bFsOff = 0x1,
    .config.whitenMode = 0x2,
    .__dummy0 = 0x00,
    .txWord = 0xABCD,
    .__dummy1 = 0x00,
    .endTrigger.triggerType = 0x1,
    .endTrigger.bEnaCmd = 0x0,
    .endTrigger.triggerNo = 0x0,
    .endTrigger.pastTrig = 0x0,
    .syncWord = 0x930B51DE,
    .endTime = 0x00000000,
};

  • Hi Vikas,
    It is recommended to start with TI-RTOS example and export SmartRF studio settings for 50kbps 2-GFSK mode at 915MHz and implement the following overrides:

    In addition to applying the wb_dsss patch change the following:

    MCE_RFE_OVERRIDE(1,0,0,1,0,0),// WB-DSSS MCE, GFSK RFE patch
    HW_REG_OVERRIDE(0x6088,0x410E),//change AGC override

    DSSS overrides:
    HW_REG_OVERRIDE(0x52AC,0xB03),//0xB03 for DSSS = 4, K = 4; 0x0800 for DSSS = 1; 0x0900 for DSSS = 2; 0x0F33 for DSSS = 8
    HW_REG_OVERRIDE(0x5108,0x0048),//correlator threshold for sync

    modify CMD_PROP_RADIO_DIV_SETUP :
    .modulation.modType = 0x0,
    .modulation.deviation = 0x2BC,
    .symbolRate.preScale = 0xF,
    symbolRate.rateWord = 0x50000, //500kbps
    .rxBW = 0x2F,
    .formatConf.nSwBits = 0x20,
    .formatConf.bMsbFirst = 0x0,
    .formatConf.fecMode = 0x0,

    modify CMD_PROP_TX and RX:
    .syncWord = 0x333C3C33, // you can change this

    Note that we are presently characterizing the WB-DSSS for other DSSS settings and the parameters above may slightly change. The above configuration, however, should work fine with sensitivity of -106dBm.
  • Hello FI,
    Thank you for your valuable inputs. One thing i want to ask why did you change the symbol rate to 500 kbps. Is it mandatory or we can keep it to 50 kbps.
    And one thing more what do you mean by OTHER DSSS SETTINGS. Please let me know.
    Thanks & regards
    Vikas
  • Hi Vikas,
    Yes, changing to 500kbps is required because that is the over-the-air data rate.
    The other DSSS settings are the DSSS codes that are assigned to the bitstream corresponding to 1 and 0. Higher DSSS settings (2,4,8) reduce the effective bitrate according to symbolrate/(2*DSSS). E.g for DSSS = 4 the effective bitrate is (500/2/4) = 62.5kbps.
    Also, higher DSSS settings will give better sensitivity.
    Note: Over-the-air datarate will remain 500kbps for all DSSS settings.
  • Hi FI

    Thank you  for acknowledging. Is there any restriction with frequency. Can i use this settings for 433-527 Mhz band.

  • Hi,
    I have not tested this frequency band but I don't think this should be a problem from the modem point of view. You still need to proceed from SmartRF studio by changing the frequency to 433MHz and exporting the settings. This will change the .loDivider in the Prop_Radio_Div setup to 0x0A.
    Also, you have to make sure the front end filter is optimized for 433MHz band.
  • Is there any specific reason behind selecting over the air data rate to 500 kbps?

  • Hi,
    FCC15.247 requires that the 6dB bandwidth be greater than 500kHz for non frequency hopping digital systems. Hence the need for 500kbps datarate.