This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1201: Matching impedance of RF ports to separate 50 ohm PA and LNA at 270-320 MHz.

Part Number: CC1201

I need to match the impedance of the LNA input and PA output on CC1201 @ 270-320 MHz to separate 50 ohm sources and loads respectively.

I have designed the attached schematic 

Is this right?

Thanks in advance.

Bruno B.

  • Hi Bruno,

    I'm not able to see your schematics. Can you upload a .pdf-file using the insert attachment functionality?

    Thanks,
    Simon

  • 6036.894-06-01_sch.pdfHi Simon.

    Hope you can see the attached pdf.

    Thanks.

    Bruno B.

  • Ok.
    I have uploaded the file 894-06-01_sch.pdf.

    Thanks again.
    Bruno B.
  • Just a few comments:

    With reference to www.ti.com/.../swra398a.pdf there are some component values that should be changed.
    C174 = 39 pF
    C176 = 1.0 pF
    C175 = 3.0 pF
    C173 = 56 pF

    Not sure about the PI capacitor network you have connected towards the UFL's. Use series dc blocking capacitor towards both UFL's.
  • Hi Simon.

    Thanks for your responce.

    I will try you suggestions.

    BTW I missed to tell you that I have already produced the prototypes and the performances of the TX path are ok for me.

    I have some issues in the RX PATH. Sensitivity is not good.

    About C62 and C181: they are not PI cap network. They are a single cap that can be mounted in 3 different positions.

    In this way I can measure different paths in the circuit.

    Attached you can find the PA section and the LNA section I have designed.

    Thanks again.

    Bruno B.

  • Have you verified that the LNA part of the RF path gives the wanted performance?
  • Hi Simon.

    I have measured the sensititvity of the transceiver and it seems to be right: I have about -93/-95 dBm sensitivity @ 500 kbps.
    The LNA section (antenna filter, TX/RX filter, attenuators, LNA and SAW filters) have a GAIN of 25 dB and it is ok.
    The combination of the two does not have the wanted performance. I guess that is a Noise issue; I mean: the NF of the RX path seems to be very poor.
    I will investigate more this issue.

    Thanks and Best Regards.
    Bruno B.
  • What is the sensitivity you see for the full system and what do you expect?
  • Hi TER.

    I measure a sensitivity of about -80 dBm for the full system.

    With reference to the attached pdf I have made the following considerations:

    RX_PATH.pdf

    RX PATH (excluding CC1201) Noise Factor Calculation

    IL dB NF dB F Att G G dB
    ANT BPF 1 1 1,2589254118 1,2589254118 0,7943282347 -1
    TX/RX SWITCH 0,3 0,3 1,0715193052 1,0715193052 0,9332543008 -0,3
    ATTEN 1,5 1,5 1,4125375446 1,4125375446 0,7079457844 -1,5
    LNA -30 1 1,2589254118 0,001 1000 30
    SAW + SWITCH 3,2 3,2 2,0892961309 2,0892961309 0,4786300923 -3,2
    TOT 24
    F1 1,2589254118 G1 0,7943282347
    F2 1,0715193052 G2 0,9332543008
    F3 1,4125375446 G3 0,7079457844
    F4 1,2589254118 G4 1000
    F5 2,0892961309 G5 0,4786300923
    Gtot 251,188643151
    RX PATH Noise Factor F (Friis Formula) 2,40090853
    RX PATH Noise Figure NF 3,8037561459
     
    Noise Floor Calculation for CC1201 without RX PATH
    k Boltzmann T Kelvin BW Hertz P(dBW) Noise Floor dBm Sensitivity dBm
    1,38E-023 290 1 -203,977229157 -173,977229157 -95
    1,38E-023 318 833333 -144,3687521338 -114,3687521338 CNR dB
    7
    Noise Figure of CC1201
    Using Equation 

    Sensitivity (dBm) = Noise Floor + CNR = -174 + 10 log B + NF + CNR

    where CNR = Carrier-to-Noise Ratio

    and assuming a desired CNR = 7dB (verified by Spectrum Analyzer readings), a Noise Floor of -114 dBm @ 45 °C (318 K) and a CC1201 Sensitivity of -95 dBm (as stated by data-sheet for 833 kHz RBW and verified by real measurement), we have:
    Sensitivity (dBm) = Noise Floor + NF + CNR
    NF = Sensitivity (dBm) - Noise Floor – CNR = 12,3687521338
    F = 10^(NF/10) = 17,253420751
     
    Noise Floor Calculation for RX PATH
    k Boltzmann T Kelvin BW Hertz P(dBW) Noise Floor dBm
    1,38E-023 290 1 -203,977229157 -173,977229157
    1,38E-023 318 833333 -143,5769379361 -113,5769379361
    NOISE FIGURE of Complete RX PATH (including CC1201)

    Ftot = F_rxpath + (F_CC1201 -1)/G_Rxpath

    = 2,4656145635
    NFTOT = 10log10(F) = 3,919251866
    Sensitivity of Complete RX PATH
    Sensitivity (dBm) = Noise Floor + NF + CNR = -102,6576860701

    So I expect a sensitivity about -100 dBm.

    Maybe something is wrong?

    Thanks again.

    Bruno B.

  • Hi Sverre.

    Thanks for your comments.

    What's about L193? Is it better to mount a 0 Ohm.

    Thanks.

    Bruno B.