Hi, I´m using CC1310 Launchpad V1.4, flashed with C:\Program Files (x86)\Texas Instruments\SmartRF Tools\SmartRF Packet Sniffer 2\sniffer_fw\bin\cc13x0lp\sniffer_fw.hex.
The led is blinking.
Running under Windows 10, SmartRF Packet Sniffer 2 V 1.04.00
The Sniffer Agent reports always "Sniffer Device Not Found"
When connected to PC the Launchpad is detected as a COMM PORT.
I have not tested with other OS, but as viewed in other questions on the forum, W10 apparently is not the problem.