I have been struggling to get more than a 1000 feet or so of range using my cc1350 launchpads with an external 1/4 wave 50ohm antenna. I attached an external antenna booster that amplifies about 10x and was able to get about a 1/2 mile. I am looking at the RF voltage output from the mcu going into 50 ohms and it looks like it is only around 20 millivolts. That equates to -20 dBm or so which is pretty much what I see as the RSSI value when receiving with another launchpad if it is right next to the one transmitting. I have programmed the simplelink power to 10. Is this not dBm? Does anyone know what the expected voltage peak is for a cc1350 at 915Mhz into 50 ohms when TX power is set to 10? I expected waveform peaks of 1V. Is there something I don't understand? Thanks for any insights.