This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
We are using HSM and the example rfPacketErrorRate for our hardware benchmark. I wonder whether the HSM can support 1Mbps. This idea come from what I have read this document Achieving Optimum Radio Range (Rev. A), on page 10 where it has the sensitivity -97dBm measured at 1Mbps for CC13xx.
If 1Mbps support is possible, how about 2Mbps? Since we are facing a challenging design issue on our hardware to achieve better sensitivity level, and if running at 1 or 2Mbps is possible by only software change it can help us a lot.
Thanks for help.
Hello,
HSM mode on CC1310 refers to 4mbps fixed datarate with 8FSK modulation. It is possible to achieve 1mbps datarate 2(G)FSK and upt0 1.5mbps 4(g)FSK (programmable datarate) on this device as well in the 868/915MHz bands. Please refer to the following posts for settings needed for these modes.
Regards,