Other Parts Discussed in Thread: CC1310
Hi,
We are looking for a RF design; with range extender based on CC1310 - CC1190 in 433.05 - 434.79 MHz range.
In device control panel of SmartRF studio, for the following configuration the maximum possible transmit output power is 13 dBm. Our expected range between two devices is 400m.
Target Configuration:
RF Design Based On: LAUNCHXL-CC1310-CC1190
Settings for 431-527 MHz band
Also do you suggest any other front end module for range extension with CC1310 mcu.
Thanks,
Ijaz