This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1150: CC1150 frequency shift,

Part Number: CC1150


Hi,

One of our custom product using CC1150 has some issue with the frequency shifting to 600Khz from 920MHz.
The occurance of this issue is very rare and also it occurs with different temperature.
Occured once at -17 deg and once at +65 deg. Out of 10K boards only one board has this issue.

Just wanted to clarify if this kind of issue (shift in the frequency) could be related to the 26MHz crystal?
CC1150's errata doesn't seems to be related to this kind of frequency shift issue.

Best Regards
paddu