This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: EOL capacitor alternatives

Part Number: CC1310

Murata announced EOL on the follow capacitors, and possible other ones, that are used in the CC1310 reference design for the VDDS_DCDC and DCOUPL pin decoupling.

GRM188R71E104KA01D  - CAPACITOR, CERAMIC X7R, 100nF, 25V, -10%/+10%, -55DEGC/+125DEGC, 0603, SMD

GRM155R61A105KE15D - CAPACITOR, 0402 1UF 10VOLTS X5R 10%

I am concerned that there are specific requirements for these capacitors that may impact the operation of the 1310.

Are there TI approved alternatives for these?

Does GRM188R71E104KA01D need to be rated at 25V?

Does GRM155R61A105KE15D need to be 1uF?