This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: Is rfEasyLinkNp sample code compatible with rfWsnConcentrator sample?

Part Number: CC1310

I want to use the concentrator sample code and add a few nodes.

The combination of the rfWsnNode and rfWsnConcentrator work perfectly, however adding a serial task, together with a FSM for a protocol seems like a lot of work.

Could anyone tell me if the rfEasyLinkNp sample code (AT-command demo) works together with the rfWsnConcentrator?

Or otherwise how to set up a task for the UART so I can assemble my payload for the communication and pass that on to the RF communication task?

Regards,

Roland