This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compatibility of the Coprocessor application with a Pi Zero

Part Number: CC1310

Tool/software: Linux

We have successfully managed to run the coprocessor appliction on a Pi 3B and are trying to do the same with a Pi Zero, however when we try to run the application the following error is given:

Unknown Host type: armv6l
Expected: armv7l {for BBB}
Expected: x86_64 {for Linux 64bit host}

The application runs as expected on the Pi 3B .

cat /proc/cpuinfo output on the Pi 3B:

processor    : 0
model name    : ARMv7 Processor rev 4 (v7l)
BogoMIPS    : 38.40
Features    : half thumb fastmult vfp edsp neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm crc32
CPU implementer    : 0x41
CPU architecture: 7
CPU variant    : 0x0
CPU part    : 0xd03
CPU revision    : 4

processor    : 1
model name    : ARMv7 Processor rev 4 (v7l)
BogoMIPS    : 38.40
Features    : half thumb fastmult vfp edsp neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm crc32
CPU implementer    : 0x41
CPU architecture: 7
CPU variant    : 0x0
CPU part    : 0xd03
CPU revision    : 4

processor    : 2
model name    : ARMv7 Processor rev 4 (v7l)
BogoMIPS    : 38.40
Features    : half thumb fastmult vfp edsp neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm crc32
CPU implementer    : 0x41
CPU architecture: 7
CPU variant    : 0x0
CPU part    : 0xd03
CPU revision    : 4

processor    : 3
model name    : ARMv7 Processor rev 4 (v7l)
BogoMIPS    : 38.40
Features    : half thumb fastmult vfp edsp neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm crc32
CPU implementer    : 0x41
CPU architecture: 7
CPU variant    : 0x0
CPU part    : 0xd03
CPU revision    : 4

Hardware    : BCM2835
Revision    : a22082
Serial        : 000000001499d059

cat /proc/cpuinfo output on the Pi Zero W

processor    : 0
model name    : ARMv6-compatible processor rev 7 (v6l)
BogoMIPS    : 697.95
Features    : half thumb fastmult vfp edsp java tls
CPU implementer    : 0x41
CPU architecture: 7
CPU variant    : 0x0
CPU part    : 0xb76
CPU revision    : 7

Hardware    : BCM2835
Revision    : 9000c1
Serial        : 0000000096138330

Is there a workaround we can use to run the coprocessor application on the Pi Zero W?