This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1350STK: data transfer from CC1350 STK to esp32 via bluetooth

Part Number: CC1350STK
Other Parts Discussed in Thread: CC1350,

Hi,

    using the  link given below( at bottom end ) we have tried porting simple peripherial cc1350 launchpad to cc1350 sensor tag.

1)I have included Board.h file in my project as shown in bottom picture.

  

2)I have also included cc1350stk.c and .h file in my project. i didnot find exclude from build option for cc1350_LAUNCHXL.c file since this file was found under includes.

3) I have included CC1350STK_7XS and  replaced CC1350_LAUNCHXL to CC1350STK as shown in bottom picture.

4) I have cleaned my project, in that it shows that it could not find simple_peripheral.obj , simple_peripheral.d , ECCROMCC26XX.obj,   Display.obj , Display.d , TRNGCC26XX.obj , TRNGCC26XX.d , 

board.obj, board.d, icall.d, ble_user_config.obj , ble_user_config.d  , devinfoservice.obj ,devinfoservice.d .   Should i include all these .obj and .d files from some other project into this simple peripheral project directory?

5) then i have rebuild my project then it shows  as bottom picture

6) i have included my application code in main.c .    How to get rid of these errors

Thanks in advance.

e2e.ti.com/.../658662

  • Hi cheekatla,

    Which SDK version are you using? There are directions for porting an SDK project to a custom board included in the BLE user's guide that I believe could be used as a guide for what you are doing, e.g. this is the guide for CC13x0 SDK 2.10.00.36: dev.ti.com/.../index.html

    Regards,
    Katie
  • Hi cheekatla,

    I'm going to close the thread due to inactivity, but you can still post back if you have more information and are still having issues and we'll be glad to help!

    Regards,
    Katie
  • Hi Kaite,

    I  have ported launchpad to stk as per the steps in that link. I cloned a new directory named my board and changed launchxl files to myboard and then removed launchxl.c and launchxl.h and added  cc1350stk.

    I changed link directory on required .h files.  From board.h file  i  selected  rf config and then defined that  rf config in bleuserconfig files. I have Included CC1350STK in preprocessor include.Now i am getting following

    errors. Thanks in advance.

    Cheers,

    Ram