This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1350: BTool -Device reset time out error

Part Number: CC1350
Other Parts Discussed in Thread: CC2650

After programming the host_test_cc1350lp_app  I get the following message when trying to communicate with the cc1350 board.

Please advise. 

1] : <Info> - 10:10:50.574
Port opened at 7/16/2018 10:10:50 AM
--------------------------------------------------------------------
[2] : <Tx> - 10:10:51.963
-Type : 0x01 (Command)
-OpCode : 0x0C03 (HCI_Reset)
-Data Length : 0x00 (0) byte(s)
Dump(Tx):
0000:01 03 0C 00 ....
--------------------------------------------------------------------
[3] : <Error> - 10:10:53.988
Message Response Timeout
Name = HCI_Reset
OpCode = 0x0C03
Tx Time = 10:10:51.963
--------------------------------------------------------------------
[4] : <Warning> - 10:10:54.014
Device Reset Timeout
Device May Not Function Properly
--------------------------------------------------------------------