This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: TI latest Uniflash cloud version can't load image

Part Number: CC1310
Other Parts Discussed in Thread: UNIFLASH,

I use uniflash online cloud version, and then use TI XDS110 to load program, I have installed the latest TI XDS driver(Emulation package 8.0.27.9), but found no way to load the program into my CC1310 boards, click verify image prompts error:

[ERROR]Cortex_M3_0:File Loader:Verification failed:Values at address ... do not match Please verify target memory and memory map.

click load image prompts error:

[ERROR]Cortex_M3_0: GEL: Error while executing OnFileLoaded(0,0): Could not read 0x50001318: target is not connected at _deviced = *(unsigned int)0x50001318[cc26x0.gel:96] at LoadTirtosRomSymbols() [cc26x0.gel:84] at OnFileLoaded(0,0).

 

So, What is the reason for this?

  • Hello,

    I would recommend downloading flash programmer 2 and doing a mass erase of the chip and try to flash the device using flash programmer and see if this helps.

    Regards,
    AB
  • Flash programmer2 can load program, but I wanted to generate a command line tool packege for all deployment platforms from the Uniflash cloud version. And then I try to load program before generating CLI packege, and appear this problem.
    In the previous version (Emulation package 7.0.188.0), I have generated CLI packege and the online program is also no problem.I don't know why the latest version (Emulation package 8.0.27.9) appeared this problem.
  • Hello User,

    We tried re creating this issue and could not. Can you provide more information or were you able to fix this problem?