This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC1310: 15.4-stack Long range mode SDK 2.20.00.38 not working

Part Number: CC1310

Tool/software: TI-RTOS

Hi,

When using TI 15.4 stack SDK 2.10.... the long range mode(5kb/s) was working fine.

When moving to 2.20.00.38 we cannot get it to work. Simplest test is to use to co-processor devices and setup network with that.

Problem is that the association request never is received on concentration. (does not indicate this on UART) 

My external script is the same that worked well for 2.10.00.36 SDK and earlier versions.

I have seen no change log to indicate changes in API in stack...

Regards

ON