I Know that to manage the power ramp I can use 2 register :
a)PA_CFG1 with the selection of the first IPL and of the Second IPL to make a shape of the spectrum.
b)PA_CFG2
The power output will be setted in a fine way , using
the output power are:(PA_POWR_RAMP+1)/2 -18dbm
There are 3 corsare value: 0x0 0x01 0x02....
Is possible to start the ramp-up curve frome one of this point? ( from one of this power level ? ) NOT ONLY FROM LEVEL PA_POWER_RAMP=3 ?
Is there a circuit for managing the power ramp that can be conveniently used?
There is an external circuit that will help ?
Best Regards
Novello G