Hi all,
I am encountering an error while flashing firmware onto a CC1310F128. It says the debug interface is locked. As such, I followed the instructions to do a mass erase and was able to successfully flash an image onto the CC1310.
However, without closing the program, when I try to flash firmware onto another CC1310F128, I am getting this error:
I am unable to connect or do a mass erase unless I close the program and relaunch Flash Program 2. When I do a refresh, it says the debug interface is locked and I can do mass erase again. I have a few hundred CC1310 to flash and all of them have the debug interface locked somehow. I can't possibly be closing and re-launching Flash Programmer 2 every time. Anyone know what is wrong and how can I flash the firmware without having to close and reload the program everytime.
Thanks in advance.